I2C Bus extender P82B715

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Bus extender P82B715

Jump to solution
736 Views
ashno_james
Contributor I

Hi All,

We are using P82B715 for connecting multiple slaves with one master MCU to compensate Bus capacitance ( in certain cases we have to connect upto 16 slaves, and we have to go with same design for MCU board , that is why we are using Bus Extender). In our case GND will be same for both Slave PCB board and Master ( MCU) PCB board. But the power supply generated for both boards are from different sources of same voltage output  levels (5V).  Sample Schematic attached.

Can you please comment on this power supply scheme, whether it is OK or not for proper I2C communication functionality ( speed is 100KHz)?

And How about two slaves in the slave PCB board which shares the Sx,Sy lines  ( SDATA, SCLK) and is pulled up to different power supply's  ( one LDO and a Buck regulator) of same voltage output (5V), and sharing common GND.

 

Thanks& Regards

0 Kudos
1 Solution
730 Views
reyes
NXP TechSupport
NXP TechSupport

Since the voltage level is the same, you should not have any communication issue using this configurations, otherwise, you would need to use a logic level shifting by using an external transistor as in Figure 10 of the App Note AN10710: https://www.nxp.com/docs/en/application-note/AN10710.pdf.

View solution in original post

0 Kudos
1 Reply
731 Views
reyes
NXP TechSupport
NXP TechSupport

Since the voltage level is the same, you should not have any communication issue using this configurations, otherwise, you would need to use a logic level shifting by using an external transistor as in Figure 10 of the App Note AN10710: https://www.nxp.com/docs/en/application-note/AN10710.pdf.

0 Kudos