I would like to see example code for t1042

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I would like to see example code for t1042

1,336件の閲覧回数
namhoon-Hwang
Contributor I

Dear nxp staff,
hello.My name is Nam-Hoon Hwang, a researcher at Shinbo.
I want to develop using nxp's t1042 chip, where can I find example code?
Let's take a look at the overall function through the example code.
If you know, please attach a link or file.

thank you.

Email Address : [email protected]

0 件の賞賛
返信
1 返信

1,311件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could download and refer to QorIQ Linux SDK 2.0, please refer to https://www.nxp.com.cn/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf.

Please download and install ISOs "Source: QorIQ Linux SDK v2.0" and "Cache: QorIQ Linux SDK v2.0 PPCE5500 Yocto" in the same path from https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk....

$ source ./fsl-setup-env -m t1042d4rdb

$ bitbake u-boot -c patch -f

Get u-boot source code in build_t1042d4rdb/tmp/work/t1042d4rdb-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git/

$ bitbake virtual/kernel -c patch -f

Get Linux Kernel source code in build_t1042d4rdb/tmp/work/t1042d4rdb-fsl-linux/linux-qoriq/4.1-r0/git/.

 

0 件の賞賛
返信