How to modify dts to make sure the M7 and A53 work ok for S32R45

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to modify dts to make sure the M7 and A53 work ok for S32R45

550 Views
aiweixin
Contributor IV

Hi,

    I want to start up both M7 and A53 core, M7 run user app, and A53 run linux.

    I find a issue: the M7 start firstly,and initialize gpio56, then control the led flashing; when A53 load linux and dtb, the linux also initialize gpio56(siul2), which cause the user app on M7 work failure.

    How can i do for it? Some doc or idea? 

aiweixin_0-1677231320829.png

 

aiweixin_1-1677231967145.png

Tags (2)
0 Kudos
Reply
2 Replies

517 Views
UrikRodriguez
NXP Employee
NXP Employee

Hello @aiweixin ,

Could you please share me how did you start the M7 core?

It is likely that what is happening to you is that the mmc dev ${mmcdev} command reconfigures the pins for the uSDHC (among another configurations), which are the ones you use to toggle the LED. You can start the M7 after running the mmc dev command but this could cause problems with the A53 application. 

 

Best regards, 

Urik

0 Kudos
Reply

519 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have passed your question to the RADAR SW team.

Best regards,

Peter

0 Kudos
Reply