Currently, I am using S32R294.
and I want to download the external flash of S32R294 from S32 Design Studio for Power Architecure.
As I know, the code of external flash is copied to SRAM when boot because there is no internal flash in s32r294.
Could you please let me know and the document for the above two item?
BRs.
Hyunung Park
Solved! Go to Solution.
Hello,
Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.
So you only then need to read RAM in your debug session.
There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.
Best regards,
Peter
Hello,
Boot ROM downloads the entire application image structure to the RAM address defined by the RAM start pointer in the image
structure.
So you only then need to read RAM in your debug session.
There is no document describing this process besides reference manual. Refer to Chapter 8 System Boot.
Best regards,
Peter