Hi,
I have created a Blob Image for S32R45, the Blob image contains a project "Siul2_Port_ToggleLed_S32R45_M7", which can make LED0 to flashes on S32R45 EVB.
When i download the Blob Image to flash, and RCON is configured to boot from QuadSPI, but the LED0 no response.
I only develop the code of bootloader app, but the IVT contains Multiple images(DCD, HES, boot app, etc.). How to debug it and confirm the stage that BootROM run at abnormally?
Currently, I have Lauterbach debugger and S32 Debug Probe, can they debug IVT or Blob Image? If they can, how to use them to debug?
Best Regards!
Hello,
I am not sure what to answer here.
Since you are not able to debug with Luaterbach, I assume there is some restriction to access your image in memory.
Could you ask Lauterbach if there are any configurations which need to be set?
Best regards,
Peter
Hi Peter,
I am trying to debug with Luaterbach.
Because I don't understand much about this tool, i will ask Lauterbach.
Best regards!