How to creating and using own Lib with CW?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to creating and using own Lib with CW?

Jump to solution
2,034 Views
wwx
Contributor I

The hardware platform used for project development: MPC5xxx
Project development using the IDE: CW for MPC5xx

After a few days of research, and did not find static library related options in CW for MPC55xx.

0 Kudos
Reply
1 Solution
1,858 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

it is possible to create static library using CW for MPC55xx, MPC56xx 2.10. Create new project, open project settings and click EPPC Target. On the top of this page, there a menu which allows you to choose Library. Please see the figure below:

pastedImage_1.png

If you have any other questions, please feel free to write me back.

Regards,

Martin

View solution in original post

0 Kudos
Reply
1 Reply
1,859 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

it is possible to create static library using CW for MPC55xx, MPC56xx 2.10. Create new project, open project settings and click EPPC Target. On the top of this page, there a menu which allows you to choose Library. Please see the figure below:

pastedImage_1.png

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 Kudos
Reply