How to copy code from FLASH to DDR2 in MPC8568?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to copy code from FLASH to DDR2 in MPC8568?

Jump to solution
1,047 Views
jalal
Contributor I

Hi my friends,

How can i copy my code from FLASH to DDR2 (after startup and boot from FLASH) and then run my code from DDR2 in MPC8568?

Thanks.

Tags (1)
0 Kudos
Reply
1 Solution
895 Views
morel_hunter1
Contributor II

/*
 * Based on default linker command file for PPC EABI
 * ROM/SRAM (L2) target
 * TEXT copied from ROM to RAM, section .text
 */

// **NOTES:
// - ROM Image address setting in linker preference panel must
//    match the address of the rom memory segment (below).

MEMORY {
    // *** Check project linker settings for stack location when adjusting RAM
    ram    : org = 0x00002000, len= 0x7E000  // SRAM: Firmware use, 512KB @ 0x0

    // *** When changing rom origin, also change EPPC Linker->ROM image for debug session
    rom    : org = 0xfff80000, len= 0x7f000  // application start ROM address
    rom_4k : org = 0xfffff000, len= 0x1000   // initialzation/reset section
}

FORCEACTIVE { gInterruptVectorTable, __reset }

SECTIONS {
   
    .app_flash : {
        *(.intvec)
        *(.rdata)
        *(.rodata)
        *(.ctors)
        *(.dtors)
        *(extab)
        *(extabindex)
    } > rom
   
    GROUP : {
        .text (TEXT): {}
        .data : {}
        .sdata : {}
        .sbss : {}
        .sdata2 : {}
        .sbss2 : {}
        .bss : {}       
        .PPC.EMB.sdata0 : {}
        .PPC.EMB.sbss0 : {}       
    } > ram
   
   
    GROUP : {
        .= 0xFFFFF000;
        .init LOAD(0xFFFFF000): {}
        .= 0xFFFFFFFC;
        .reset LOAD(0xFFFFFFFC) : {}
    } > rom_4k    
                   

    // The dummy section is just a placeholder.  The linker automatically
    // generates an address for it in the ROM image, which tells us
    // where the end of the ROM image is.

    .dummy : {}

    // 4 MB FLASH, 2 MB x 16
    ___FLASH_START  = 0xFFC00000;
    ___FLASH_SIZE   = (4 * 1024 * 1024);

    // Application flash
    ___APP_START    = ADDR(.app_flash);
    ___APP_SIZE     = SIZEOF(.app_flash);
       

}

 

View solution in original post

0 Kudos
Reply
3 Replies
895 Views
morel_hunter1
Contributor II

I develop with Code Warrior and direct the linker to locate executable in DDR or SRAM. The linker directives and CW library takes care code location (ROM -> RAM) and data init.

0 Kudos
Reply
895 Views
jalal
Contributor I

Hi

 

Would you mind tell me how can i do it? Can you send linker file to me?

 

Thanks for your guidance

0 Kudos
Reply
896 Views
morel_hunter1
Contributor II

/*
 * Based on default linker command file for PPC EABI
 * ROM/SRAM (L2) target
 * TEXT copied from ROM to RAM, section .text
 */

// **NOTES:
// - ROM Image address setting in linker preference panel must
//    match the address of the rom memory segment (below).

MEMORY {
    // *** Check project linker settings for stack location when adjusting RAM
    ram    : org = 0x00002000, len= 0x7E000  // SRAM: Firmware use, 512KB @ 0x0

    // *** When changing rom origin, also change EPPC Linker->ROM image for debug session
    rom    : org = 0xfff80000, len= 0x7f000  // application start ROM address
    rom_4k : org = 0xfffff000, len= 0x1000   // initialzation/reset section
}

FORCEACTIVE { gInterruptVectorTable, __reset }

SECTIONS {
   
    .app_flash : {
        *(.intvec)
        *(.rdata)
        *(.rodata)
        *(.ctors)
        *(.dtors)
        *(extab)
        *(extabindex)
    } > rom
   
    GROUP : {
        .text (TEXT): {}
        .data : {}
        .sdata : {}
        .sbss : {}
        .sdata2 : {}
        .sbss2 : {}
        .bss : {}       
        .PPC.EMB.sdata0 : {}
        .PPC.EMB.sbss0 : {}       
    } > ram
   
   
    GROUP : {
        .= 0xFFFFF000;
        .init LOAD(0xFFFFF000): {}
        .= 0xFFFFFFFC;
        .reset LOAD(0xFFFFFFFC) : {}
    } > rom_4k    
                   

    // The dummy section is just a placeholder.  The linker automatically
    // generates an address for it in the ROM image, which tells us
    // where the end of the ROM image is.

    .dummy : {}

    // 4 MB FLASH, 2 MB x 16
    ___FLASH_START  = 0xFFC00000;
    ___FLASH_SIZE   = (4 * 1024 * 1024);

    // Application flash
    ___APP_START    = ADDR(.app_flash);
    ___APP_SIZE     = SIZEOF(.app_flash);
       

}

 

0 Kudos
Reply