How to clear the Access error frame in MC33774

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to clear the Access error frame in MC33774

625 次查看
Chandru_8051
Contributor I

Uc : ST controller

Chipset: MC33774A(SPI Version)

I can able to read and write successfully. While reading some of registers, The received data is with Access error frames. Framed packet is fine and working for the other registers but the same method is not working for some of the msg frames. For example, I tried to read the analog status and communication fault status register, communication fault succeeds and  analog fault status of messages contains 0x3FFF as register field.(Sample received data image is attached within this trail)

Access frame is occured. I tried to read the valid register content(0x422) but the resultant received data in DATA0 field is 0x425. What is the cause of this issue ? Whether I need to preconfigure some contents before Either ?

 

Chandru_8051_0-1734418111019.png

 

 

标记 (1)
0 项奖励
回复
2 回复数

602 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

There is a detailed description in the MC33774A full datasheet.

Screenshot 2024-12-17 122904.png

I hope it helps.

BRs, Tomas

0 项奖励
回复

599 次查看
Chandru_8051
Contributor I
Hi Tomas, I had already gone through though. Why it responds with that frame though I had framed with the proper packet.
I also checked the AccessError Message, It has no error in the FEH_ACC_Err
0 项奖励
回复