How to add C++ file in SDRAM section using MCUXPresso Linker script

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add C++ file in SDRAM section using MCUXPresso Linker script

2,073件の閲覧回数
emb02
Contributor V

Hi,

I'm using MIMXRT1021 evaluation board in which I want to put the entire C++ file into external SDRAM.

In MCUXpresso project settings there is one option to Manage Linker script but I'm not getting any reference to add file into SDRAM section.

I've tried but not able to do the same. Please guide me further.

MIMXRT.PNG

0 件の賞賛
返信
6 返答(返信)

2,026件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @emb02 ,

Hope you are doing well!

This post should meet your needs, please refer to it: https://mcuoneclipse.com/2021/05/26/placing-code-in-sections-with-managed-gnu-linker-scripts/

 

Best regards,
Gavin

0 件の賞賛
返信

2,022件の閲覧回数
emb02
Contributor V
Hi,
I've tried this way but my MIMXRT1021_Project_Debug.ld file does not update after doing this steps.
0 件の賞賛
返信

2,018件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Is your *.cpp file in the source folder? This should be necessary.

0 件の賞賛
返信

2,014件の閲覧回数
emb02
Contributor V

Hi,
Yes my Test1.cpp file is in the source folder.
Can you verify - */Test1.o (.text .text*)
Is this the correct way of adding file name?

0 件の賞賛
返信

1,921件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @emb02 ,

On my side, I have implemented a method to put a C file into SDRAM. Please refer to <MCUXpresso IDE User Guide> Chapter 20.13.5 Placing specific functions into RAM blocks.

Gavin_Jia_0-1713522954031.png

// test.h

#ifndef TEST_H_
#define TEST_H_

#ifdef __cplusplus
extern "C" {
#endif

#include <cr_section_macros.h>
__RAMFUNC(RAM2) void my_function(void);

#ifdef __cplusplus
}
#endif

#endif /* TEST_H_ */

Hope it helps!

Best regards,
Gavin

0 件の賞賛
返信

1,958件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @emb02 ,

Thanks for your feedback!

I'll test it for you on my end and get back to you in a timely manner. It may take some time because of the recent backlog. Thanks in advance for your kind understanding!

Best regards,
Gavin

0 件の賞賛
返信