How many bytes of data can I read at once with SC18IM700 UART-to-I2C bridge IC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many bytes of data can I read at once with SC18IM700 UART-to-I2C bridge IC?

1,189 Views
BrarP
Contributor I

Hi,

I want to integrate the SC18IM700 UART-to-I2C bridge IC in my design. At the moment, I am in the process of testing it. A diagram of my testing setup is attached below.

In my testing, I have been able to read 32 bytes of data at once with the default IC settings. Is it possible to read more bytes of data at once? I would like to read 72 bytes in one go. 

Also, is it possible to read data from a specific address with this IC? It is not mentioned in the datasheet.

Any help is much appreciated.

Thank you so much for your time in advance.

Regards,

Paul

 

 

Tags (1)
0 Kudos
3 Replies

1,150 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

For read from slave device, you can't read 72 bytes in one time, only can read N byte from slave device (N=16 max) one time.

0 Kudos

1,133 Views
BrarP
Contributor I

Hi, 

How to read data from a specific slave address? It's not mentioned in the datasheet. I tried using the following single read I2C commands but it's not working.

BrarP_0-1635268754039.png

If you can point me in some direction that would be great. 

0 Kudos

1,124 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please check attached file help or not!