Help about mx31ads habtookit setting,thanks.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help about mx31ads habtookit setting,thanks.

2,874件の閲覧回数
young
Contributor I
I failed to flash mx31ads_redboot.bin intoNor(s71ws256nd0) using mx_HABToolkit_2.2.
Error: DDR memory init error.
DIP switches setting are as below:
Cpu board: [700-20811 rev-b]
SW2: on/on/off/on/off/on/on/off
JP22: 2-3
Using Uartc port top one.[115200 8-N-1-N]
 
Baseboard:[700-20810 rev-b]
SW1: off/off/off/on
SW2: on/on/off/on/off/on/off/on
SW3: off/off/off/on/on/on/on/off
 
Atlas [700-75812 rev-1]
S7: off/off/off/off/on/on
S8: on/off/off/off/on/off
S9: off/off/on/off/off/off
S4: off/on/off/on/off/off
S5: all off
S6: off/on/off/off
 
Pls help me and give some advice, thanks a lot!
 
0 件の賞賛
返信
4 返答(返信)

1,589件の閲覧回数
rrr
Contributor I
SW2 (BOOT) on CPU board should be 1-7 ON  and 8 OFF
0 件の賞賛
返信

1,589件の閲覧回数
young
Contributor I
I changed the sw2 on cpuboard as: on/on/on/on/on,then try again,
.MX31 HABToolkit ver 1.2
UART is using
Error!!- Reason: Download code or the Flash Program can't be executed, Check the HABType
 
i don't know how to check the habtype,pls give me advice.
 
thanks a lot!
0 件の賞賛
返信

1,589件の閲覧回数
tala
Contributor I
Hello,
 I have similar problem with flashing my i.MX31 ADS HAB toolkit ver 2.21 as what you had with the "Error! - DDR memory init error"  error. I tried it with the setting that you had as well and I still have the same problem. My originial switch settings were as fallows:
 
Baseboard:
SW1: off/off/off/on
SW2: on/off/off/on/off/off/off/on
SW3: on/off/off/on/on/on/on/off
 
CPU:
SW2: all on except 8th--> off
 
ATLAS:
SW7: off/on/off/on/on/on
SW8: off/off/on/on/off/off
SW9: off/off/on/off/on/off
S4:    off/off/on/off/off/on
S5:    all off
S6:    off/on/off/off
 
I have the same error when flashing for linux as well.
Any suggestion anyone? Thank you.
 
 
0 件の賞賛
返信

1,589件の閲覧回数
rrr
Contributor I
Sounds like you have a board w/o the HAB fuse burned. If you can connect JTAG you can verify by issuing a dump/b 0x5001c810..0x5001c814. It will read 00000001 if the HAB is burned. There is a procedure to burn the HAB yourself, but some of the boards are not capable of burning the HAB fuse. I had the same problem with my first board and had to replace the board because the HAB burning utility failed.
0 件の賞賛
返信