Hello, does the UART of LPC11U6x series MCU support 7616-3 asynchronous smart card mode?Are all UART supported?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello, does the UART of LPC11U6x series MCU support 7616-3 asynchronous smart card mode?Are all UART supported?

Jump to solution
493 Views
154049250
Contributor I

Hello, does the UART of LPC11U6x series MCU support 7616-3 asynchronous smart card mode?Are all UART supported?

The data manual of LPC11U6x series MCU does not mention, in addition, is LPC11U6x series MCU compatible with LPC11U1x series MCU software?

Looking forward to your reply, thank you!

0 Kudos
1 Solution
427 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Does the UART of LPC11U6x series MCU support 7616-3 asynchronous smart card mode? Are all UART supported?
-- Only UART0 supports the ISO 7816-3 compliant smart card interface.
1) Is the LPC11U6x series MCU compatible with the LPC11U1x series MCU software?
-- In general, they're compatible with each other, however, I'd like to suggest you refer to the application note to learn the enhanced feature of the LPC11U6x versus to the other LPC11Uxx device.

Have a great day.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
428 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Does the UART of LPC11U6x series MCU support 7616-3 asynchronous smart card mode? Are all UART supported?
-- Only UART0 supports the ISO 7816-3 compliant smart card interface.
1) Is the LPC11U6x series MCU compatible with the LPC11U1x series MCU software?
-- In general, they're compatible with each other, however, I'd like to suggest you refer to the application note to learn the enhanced feature of the LPC11U6x versus to the other LPC11Uxx device.

Have a great day.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

427 Views
154049250
Contributor I

thank you!

0 Kudos