Having a problem with an AWR model for AFT05MP075N

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Having a problem with an AWR model for AFT05MP075N

1,176 Views
jfoster
Contributor I

Hi,

I am running a Microwave office simulation for AFT05MP075N (NXP_AFT05MP075N_Level1_Rev1_SPmodel_FET2). 

I am running a simulation with a two tone excitation, each tone having a different power level. 

I am repeatedly getting an error: 

9:08:11 AM Syntax error in encrypted library at line 'FSL:VA:FSLNN2'. Please contact your library vendor for more information!

9:08:11 AM Job Failed!: NLN:Schematic 1 1.AP_HB.$FDOC_87674563.0

Has anyone faced this problem with the LDMOS models? Is there a work around? 

#ads #awr #gan #rf #model #nl‌

ldmos‌ #rf ldmos

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

940 Views
LPP
NXP Employee
NXP Employee

Comment from NXP engineering team:

There were some issues with the models that are in process of being fixed. It is my understanding that the fix was implemented today. Can we get the customer to re-download the model and try again? If we are still seeing the same errors, we can continue to investigate.


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply