Getting started for the RT1060 WiFi module is different from the latest SDK Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting started for the RT1060 WiFi module is different from the latest SDK Example

419 次查看
AKobamasa
Contributor I

The explanation for Getting started for the RT1060 WiFi module is different from the latest SDK Example.

I am trying to get WiFi to work with the help of Getting Started with the MIMXRT1060-EVK, but the file structure included in the WiFi example project installed in the IDE using the import SDK example has changed significantly. There is no app_config.h and I can't find the file defining the WiFi module to use. Is there another SDK file?

0 项奖励
回复
6 回复数

303 次查看
AKobamasa
Contributor I

Hello shaun_wu,

Thank you for responding to my question. 

I am not sure how to get that settings window. Could you let me know about it?

Best Regards

0 项奖励
回复

399 次查看
AKobamasa
Contributor I

I have an additional information for this question. I use MCUXpresso IDE v25.6.136 and have got this issue.

I check this with IDE v24.12.148 and can see the file app_config.h in the directory 'source'. So I guess this is a bug in v25. 

0 项奖励
回复

283 次查看
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @AKobamasa 

 

You could refer to following image:

shaun_wu_0-1759202547060.png

 

Best Regards

Shaun

 

0 项奖励
回复

367 次查看
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @AKobamasa 

 

new sdk is different as older version, you could refer to following guide: Examples — MCUXpresso SDK Documentation

 

Best Regards

Shaun

0 项奖励
回复

364 次查看
shaun_wu
NXP TechSupport
NXP TechSupport

Hello @AKobamasa 

 

You could find it in marco definition of project:

shaun_wu_0-1758877432684.png

Best Regards

Shaun

 

0 项奖励
回复

224 次查看
AKobamasa
Contributor I

Hello shaun_wu

I succeeded to build and run the project with this setting in MCUXpresso v25.

Thanks a lot.

 

0 项奖励
回复