General error with PN5180 receive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

General error with PN5180 receive

725 Views
Leeenka
Contributor I

Hi,

we have custom board with PN5180 connected through SPI for reading cards. I followed steps in AN12650 for ISO14443 REQA. While I wait for card to response, the GENERAL_ERROR is hit in IRQ_STATUS register after first frame. I see that it means that there is some parameter error. What that exactly mean parameter error? In which register or step? Or what I need to check?

If the card is present during the first frame I can detect and read it succesfully otherwise not.

Thank you

Tags (2)
0 Kudos
Reply
1 Reply

683 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi 

 

I would suggest you refer to the register layer for PN5180. There is a PN5180 register example

https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/full-nfc-forum-compliant-frontend-ic:PN5180...

danielchen_0-1640008489595.png

 

 

Regards

Daniel

0 Kudos
Reply