Hi,
we have custom board with PN5180 connected through SPI for reading cards. I followed steps in AN12650 for ISO14443 REQA. While I wait for card to response, the GENERAL_ERROR is hit in IRQ_STATUS register after first frame. I see that it means that there is some parameter error. What that exactly mean parameter error? In which register or step? Or what I need to check?
If the card is present during the first frame I can detect and read it succesfully otherwise not.
Thank you
Hi
I would suggest you refer to the register layer for PN5180. There is a PN5180 register example
Regards
Daniel