GD3162

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
444 次查看
Akshat_VE02376
Contributor III

Hi NXP,
Please provide a clear difference between Soft Shut down, 2LTO and Segmented Driver in GD3162 as these features are not very much clear and are a blocker for our project.

0 项奖励
回复
1 解答
430 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Akshat,

SSD uses a smaller, programmable constant sink current to switch off the IGBT/SiC. The turn-off time is increased, turn-off speed is reduced and the gate is slowly discharged. This limits the di/dt and dv/dt, reducing voltage spikes and protecting the device.

Unlike SSD, the 2LTO first reduces gate drive to an intermediate programable voltage level (for a programmable duration) before fully turning it off. This reduces the peak voltage overshoot across the power device.

The segmented drive feature allows to wave shape the turn-off current and modulate the gate impedance during turn-off, for the purposes of mitigating potentially high VCE overshoot. Segmented drive is exclusively a non-fault, non-latching mode of operation during turn-off.

More details about all these features can be found in the GD3162 datasheet.

BRs, Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
431 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Akshat,

SSD uses a smaller, programmable constant sink current to switch off the IGBT/SiC. The turn-off time is increased, turn-off speed is reduced and the gate is slowly discharged. This limits the di/dt and dv/dt, reducing voltage spikes and protecting the device.

Unlike SSD, the 2LTO first reduces gate drive to an intermediate programable voltage level (for a programmable duration) before fully turning it off. This reduces the peak voltage overshoot across the power device.

The segmented drive feature allows to wave shape the turn-off current and modulate the gate impedance during turn-off, for the purposes of mitigating potentially high VCE overshoot. Segmented drive is exclusively a non-fault, non-latching mode of operation during turn-off.

More details about all these features can be found in the GD3162 datasheet.

BRs, Tomas

0 项奖励
回复