Hi,
All faults can be cleared by writing a "1" to the corresponding bit in the associated STATUSx register. To clear the watchdog fault, make sure both HV and LV sides are properly powered, then write the WDOG_FLT bit to 1 in the STATUS2 register. See also section 12.4 of the datasheet.
At 1st powerup, if LV side is powered before HV side, a WDOG_FLT will appear, until HV side is powered. At this point, the WDOG_FLT will automatically be cleared. Note that this only happens once, i.e. if the HV side then experiences a POR event, the WDOG_FLT will be latched even when power is restored.
Regarding RESET, the following sequence should be observed:
1) enter configuration mode by setting the CONFIG_EN bit to 1 in the MODE2 register. PWM operation will be disabled, INTB stays high.
2) Write the RESET bit to 1 in the MODE2 register. INTB will go low and all registers will be reset to their default value, PWM operation is still disabled.
3) Write RESET bit to 0. INTB will go back high, and PWM operation is allowed. The configuration registers can be written at this point.
BRs, Tomas