GD3162 gate driver SC fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GD3162 gate driver SC fault

Jump to solution
588 Views
Akshat_VE02376
Contributor III

Hi NXP,
What could be the reason that INTB is going to 2.5V from 5V in the case of a short circuit fault ? Can there be any causes in SW? Any possibility ?

0 Kudos
Reply
1 Solution
574 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Is the INTB pin directly connected to the microcontroller? Please note that the INTB pin has an internal passive pull-up to VDD, and INTB reports faults with an active low signal (logic 0 indicates a fault). According to the datasheet, the INTB pin should indeed be connected directly to the microcontroller.

Could you confirm whether, when disconnecting the microcontroller from the INTB pin, the voltage remains at 2.5V in the event of a fault?

 

View solution in original post

0 Kudos
Reply
4 Replies
575 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Is the INTB pin directly connected to the microcontroller? Please note that the INTB pin has an internal passive pull-up to VDD, and INTB reports faults with an active low signal (logic 0 indicates a fault). According to the datasheet, the INTB pin should indeed be connected directly to the microcontroller.

Could you confirm whether, when disconnecting the microcontroller from the INTB pin, the voltage remains at 2.5V in the event of a fault?

 

0 Kudos
Reply
552 Views
Akshat_VE02376
Contributor III

Hi, FYI,
in our project, all the INTB pins are connected to one pin of the micro so that if any one of the gate drivers (6 gate (RH, YH, BH and RL, YL, BL) for 3 phase motor) encounters a fault, the PWM is cut off for all.
In the attached image you can see that ISENSE pin of the R-L gate driver is supposed to detect phase over current cut off through SC fault and ISEN of Y-L gate driver is supposed to detect DC over current cut off through SC fault.
In our case whenever ISEN of YL detects DC bus over current cut off, in that case INTB is going to 2.5V and when phase over current cut off occurs, then INTB is further transitioning from 2.5 to 0.
I've noted your point to disconnect INTB from micro and check the signal again.

0 Kudos
Reply
506 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello

Could you please let me know the result? Additionally, would you be able to test the INTB connected directly to the microcontroller?

0 Kudos
Reply
551 Views
Akshat_VE02376
Contributor III
And also, INTB before connecting to micro is externally given a pull-up to 5V through a 10K resistor
0 Kudos
Reply