Full-duplex transfer using NXP Flex SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Full-duplex transfer using NXP Flex SPI

1,616 Views
pibew84514
Contributor I

Hi, I've got two boards, LS1028 ardb and Hilsher netX 90.

Both of them are connected through SPI using following lines:

- SCK

- CS

- GND

- MOSI

- MISO

I also have a logic analyzer connected to see what's going on on the bus.

The SPI controller I use on the LS side is FlexSPI (spi-nxp-fspi) provides only implementation for SPI_MEM framework operations.

I tried to perform some tests to check how it works:

Here is the code of my driver

https://tutuappx.com/ Vidmate

uint8_t buf[4];

struct spi_mem_op op = SPI_MEM_OP(SPI_MEM_OP_CMD(0x80, 1),SPI_MEM_OP_ADDR(3, 0x000004, 1),SPI_MEM_OP_NO_DUMMY,SPI_MEM_OP_DATA_IN(4, buf, 1));

ret = spi_mem_exec_op(spimem, &op);if (ret) {pr_info("Cannot execute op\n");}

This is what I see on the logic analyzer:

r37x22fd526c1.jpg

As you can see on the MOSI line I have what I expect in the format: opcode | addr

The problem is that, once the Hilsher SPI is clocked it immediately sends 4 bytes on the MISO line where the first one is 0x11 (it is used to distinguish the device type).

And due to that fact - once the transfer is finished, my buf consists of the following bytes:

0x6e 0x65 0x74 0x58

so the first 4 bytes were skipped But I need them especially this first byte (0x11).

Any ideas about what goes wrong?

 

0 Kudos
Reply
2 Replies

1,580 Views
yipingwang
NXP TechSupport
NXP TechSupport

I am discussing with the AE team, will provide more update later.

0 Kudos
Reply

1,550 Views
yipingwang
NXP TechSupport
NXP TechSupport

We have following questions:
Is this customer using LSDK or have their own software?
If they are using LSDK then please ask them to run following commands on U-Boot console: 'sf probe' and 'sf read <offset> <address> <count>'
Please share the register dump of XSPI controller
Provide the schematic with wiring diagram of xspi controller and SPI?
What is the platform clock used?
Can you also share the logic analyser screen shot with data skip showing?

0 Kudos
Reply