Hello,
is your 2-wire Ethernet (100BASE-T1) to Fast Ethernet (100BASE-TX) Media Converter
RDDRONE-T1ADAP
also compatible with the slower 2-wire Ethernet 10BASE-T1S or 10BASE-T1L standard?
Best regards
Hi,
Yes, RDDRONE-T1ADAP is based on the TJA1101B Ethernet PHY, and if it is configured properly, this device is also compatible with 10 Mbit/s speed, to do this you need to configure the Speed Select bits to ‘00’ (SPEED_SELECT (MSB) = 0 and SPEED_SELECT (LSB) = 0).
Regards,
Jose