FS26 SBC init delay

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS26 SBC init delay

跳至解决方案
2,003 次查看
kjy106906
Contributor IV

Hello

I have a question regarding the FS26 SBC.

Is more delay needed in the following situations?
Standby -> SPI wake up -> delay 1.5ms -> SBC init

For 1.5ms, I referred to the phrase below in the datasheet.

SPI chip select wake-up:
– When the SPI wake up is enabled, the device wakes up with any activity on the SPI bus (transition from high to low of CSB pin).
– In case of a SPI wake up, the first SPI command is ignored, and the FS26 will be ableto respond to the subsequent SPI commands after 1.5 ms.

However, init fails with 1.5ms.
Init succeeds with 10ms.

Is there an exact delay guide?

0 项奖励
回复
1 解答
1,971 次查看
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1693985814828.png

Set this time above 7ms.

 

在原帖中查看解决方案

0 项奖励
回复
9 回复数
1,983 次查看
guoweisun
NXP TechSupport
NXP TechSupport

No fully understand you wrote:

 init fails with 1.5ms.
Init succeeds with 10ms.

Could you please give more explain?

 

0 项奖励
回复
1,973 次查看
kjy106906
Contributor IV

Yes.

Standby -> SPI wake up -> delay 1.5ms -> Sbc_fs26_Init

-> return Not Ok

Standby -> SPI wake up -> delay 10ms -> Sbc_fs26_Init

-> return Ok

 

标记 (1)
0 项奖励
回复
1,972 次查看
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1693985814828.png

Set this time above 7ms.

 

0 项奖励
回复
1,912 次查看
kjy106906
Contributor IV

@guoweisun 

SBC Standby -> SPI wake up -> delay 1.5ms -> Sbc_fs26_Init

-> return Not Ok

SBC Standby -> SPI wake up -> delay 10ms -> Sbc_fs26_Init

-> return Ok

I don't know why you are talking about RSTB time.
If I put the SBC in Standby, the SBC will not become a POR.
When MCU do SBC SPI wakeup, RSTB has already been released.

 

0 项奖励
回复
1,905 次查看
guoweisun
NXP TechSupport
NXP TechSupport

---

I don't know why you are talking about RSTB time.
If I put the SBC in Standby, the SBC will not become a POR.
When MCU do SBC SPI wakeup, RSTB has already been released.

---

After wake up SBC state machine still follow below, detail in datasheet page25:

guoweisun_0-1694074353834.png

 

0 项奖励
回复
1,895 次查看
kjy106906
Contributor IV

Yes.

It says "but maintained high during wake up from Standby" on it.

so 

SBC Standby (RSTB High) -> SPI wake up (RSTB High)-> delay 1.5ms (RSTB high) -> Sbc_fs26_Init(RSTB high) -> return Not Ok

RSTB is always high, so why is RSTB Release time and delay related?

Thank you

0 项奖励
回复
1,839 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Although RSTB is high but the state machine still follow:

Default FS_OTP Loading->LBIST DONE->ENABLE Monitoring->ABIST1 test->enter INIT FS 

0 项奖励
回复
1,808 次查看
kjy106906
Contributor IV

Very Thank you I understood

0 项奖励
回复
1,978 次查看
guoweisun
NXP TechSupport
NXP TechSupport

I think below process:

Standby -> SPI wake up -> delay 1.5ms at same time the fail safety mechanism continue to flow as below picture if no failure will stop in INIT phase  -> SBC init

 

guoweisun_0-1693984140150.png

guoweisun_1-1693984180415.png

guoweisun_2-1693984196756.png

 

0 项奖励
回复