FRDM-KL25Z source clock for UART0 in polling mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL25Z source clock for UART0 in polling mode

ソリューションへジャンプ
931件の閲覧回数
mato_cica1
Contributor II

Hi NXP Community,

Please, what source clock should I use for UART0 in polling mode on FRDM-KL25Z?
I suppose that should be MCGFLLCLK clock or MCGPLLCLK/2. If so, which on of them?

Thanks in advance,

ラベル(1)
タグ(2)
1 解決策
830件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Mato,

It is MCGFLLCLK. UART0 clock source could be the MCG PLL/FLL clock. You can see in to picture that there is no /2 divider in the path.

pastedImage_1.png

Regards,

Jing

元の投稿で解決策を見る

2 返答(返信)
831件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Mato,

It is MCGFLLCLK. UART0 clock source could be the MCG PLL/FLL clock. You can see in to picture that there is no /2 divider in the path.

pastedImage_1.png

Regards,

Jing

830件の閲覧回数
mato_cica1
Contributor II

Thanks a lot, Jing.

0 件の賞賛
返信