Hello everyone,
I can down load the FRDM-KEAZ64 SDK from NXP web, I do not know whether it has SDK or not, if you have it, could you help to send it to me, thanks.
I used develop IDE is S32DS.
Thank you for contacting NXP Technical support.
To provide you with better support, can you please be more specific with the error you receive when you try to download the software?
Also, can you please share the link that you are using to download it?
Are you download it from the following link:
https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/kea-automotive-mcu...
I just use IDE(S32DS) to creat FRDM_SKEAZ64 project, there's no correspond KEAZ64 SDK for selected. whether can select KEAZ128 SDK for SKEAZ64?
@547416104
On the other hand, I suggest you try to download the software using an incognito/ private window win Chrome/ Firefox as sometimes cookies block the option to log in properly.