I’m trying to run some sample codes, but I’m not getting success. The only example that I could run properly was the “hello” example located in the “s32v234_sdk/demos/other/hello”.
I’m using the evaluation board SBCS32V234 with the MAX9286S32V234 and the camera MXOV10635-S32V. I tried to run the examples: “isp_ov10635_quad”, “isp_ov10635_viu_s”, “ispisp_jpeg_4stream” and “demos/apps/isp_flex_frame_input”, But they all give the same message error (as in the attached file):
Failed to allocate DDR buffers.
Failed to prepare DDR buffers.
Demo failed in preparation phase.
Does anyone have any idea of what may be the problem?
Please be informed, that all support to S32V234 is done via tickets. Please open a Support Case to contact NXP Technical Support with respect to the described problem.
Best Regards,
Platon