Evaluation Board SBCS32V234

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Evaluation Board SBCS32V234

583 Views

I’m trying to run some sample codes, but I’m not getting success. The only example that I could run properly was the “hello” example located in the “s32v234_sdk/demos/other/hello”.

 

I’m using the evaluation board SBCS32V234 with the MAX9286S32V234 and the camera MXOV10635-S32V. I tried to run the examples: “isp_ov10635_quad”, “isp_ov10635_viu_s”, “ispisp_jpeg_4stream” and “demos/apps/isp_flex_frame_input”, But they all give the same message error (as in the attached file):

Failed to allocate DDR buffers.

Failed to prepare DDR buffers.

Demo failed in preparation phase.

 

Does anyone have any idea of what may be the problem?

Labels (1)
0 Kudos
1 Reply

563 Views
bpe
NXP Employee
NXP Employee

Please be informed, that all support to S32V234 is done via tickets. Please open a Support Case to contact NXP Technical Support with respect to the described problem.

 

Best Regards,
Platon

 

0 Kudos