Establishing NXP NFC Chip CLR663 communication with NFC Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Establishing NXP NFC Chip CLR663 communication with NFC Card

ソリューションへジャンプ
548件の閲覧回数
K_Salewicz
Contributor II

What is the sequence of commands necessary to establish communication between NXP NFC Chip CLR663 with NFC Card ?

0 件の賞賛
返信
1 解決策
530件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi 

I would suggest you refer to AN12657: Using the RC663 without library

https://www.nxp.com/docs/en/application-note/AN12657.pdf

You can see some code snippet initializes the RC663 to the ISO 14443 protocol, sends a REQA command and listens to the response of a tag...

 

Regards

Daniel

 

 

Regards

Daniel

元の投稿で解決策を見る

3 返答(返信)
531件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi 

I would suggest you refer to AN12657: Using the RC663 without library

https://www.nxp.com/docs/en/application-note/AN12657.pdf

You can see some code snippet initializes the RC663 to the ISO 14443 protocol, sends a REQA command and listens to the response of a tag...

 

Regards

Daniel

 

 

Regards

Daniel

498件の閲覧回数
K_Salewicz
Contributor II

Thank you very much, it worked !

0 件の賞賛
返信
525件の閲覧回数
K_Salewicz
Contributor II
Thank you very much. We will test it !
0 件の賞賛
返信