Establishing NXP NFC Chip CLR663 communication with NFC Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Establishing NXP NFC Chip CLR663 communication with NFC Card

Jump to solution
1,300 Views
K_Salewicz
Contributor II

What is the sequence of commands necessary to establish communication between NXP NFC Chip CLR663 with NFC Card ?

0 Kudos
Reply
1 Solution
1,282 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi 

I would suggest you refer to AN12657: Using the RC663 without library

https://www.nxp.com/docs/en/application-note/AN12657.pdf

You can see some code snippet initializes the RC663 to the ISO 14443 protocol, sends a REQA command and listens to the response of a tag...

 

Regards

Daniel

 

 

Regards

Daniel

View solution in original post

3 Replies
1,283 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi 

I would suggest you refer to AN12657: Using the RC663 without library

https://www.nxp.com/docs/en/application-note/AN12657.pdf

You can see some code snippet initializes the RC663 to the ISO 14443 protocol, sends a REQA command and listens to the response of a tag...

 

Regards

Daniel

 

 

Regards

Daniel

1,250 Views
K_Salewicz
Contributor II

Thank you very much, it worked !

0 Kudos
Reply
1,277 Views
K_Salewicz
Contributor II
Thank you very much. We will test it !
0 Kudos
Reply