EdgeLock SE050 OpenSSL, pkcs11-tool, and SM_Connect Failed. Status 7012

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EdgeLock SE050 OpenSSL, pkcs11-tool, and SM_Connect Failed. Status 7012

4,080 Views
peter_nt
Contributor I

Hello!

 I am trying to get EdgeLock SE050 (AN12570) to work on Raspberry Pi (both 3 and 4, OpenSSL 1.0.2 and 1.1.1).

 I am getting errors with every utility I could lay my hands on, besides the seTool from the demos, which works. Here come the details:

1. seTool (works)

 

root@raspberrypi:/home/se050_middleware/simw-top/doc/demos/se05x/seTool# /home/se050_middleware/simw-top_build/raspbian_native_se050_t1oi2c/bin/seTool genECC 0x01010101 /dev/i2c-1
App   :INFO :PlugAndTrust_v02.16.01_20200818
App   :INFO :Running /home/se050_middleware/simw-top_build/raspbian_native_se050_t1oi2c/bin/seTool
App   :INFO :Using PortName='/dev/i2c-1' (CLI)
sss   :INFO :atr (Len=35)
      00 A0 00 00    03 96 04 03    E8 00 FE 02    0B 03 E8 08
      01 00 00 00    00 64 00 00    0A 4A 43 4F    50 34 20 41
      54 50 4F
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
sss   :WARN :Object id 0x1010101 exists
App   :INFO :ex_sss Finished

 

 

2. the pkcs11-tool (does not work, fails to connect to i2c device)

 

root@raspberrypi:/home/se050_middleware/simw-top/sss/plugin/openssl/scripts# pkcs11-tool --module $PKCS11_MODULE --keypairgen --key-type rsa:1024 --label "sss:20202020"
ssse-flw: EmbSe_Init(): Entry
App   :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
smCom :ERROR:Failed writing data (nrWritten=-1).

smCom :ERROR: - Error in I2C Write.....
smCom :ERROR:phNxpEseProto7816_SendRawFrame Error phNxpEse_WriteFrame
smCom :ERROR:TransceiveProcess Transceive send failed, going to recovery!
smCom :ERROR:phNxpEseProto7816_Open failed
smCom :ERROR: Failed to Open session
sss   :ERROR:SM_Connect Failed. Status 7012
App   :ERROR:sss_session_open failed
App   :WARN :nxEnsure:'kStatus_SSS_Success == status' failed. At Line:356 Function:engineSessionOpen
ssse-flw: EmbSe_Init(): Failed to initialize
ssse-flw: EmbSe_Finish(): Entry
ssse-flw: EmbSe_Finish(): Exit
Using slot 0 with a present token (0x1)
smCom :ERROR:phNxpEseProto7816_SendRawFrame Error phNxpEse_WriteFrame
smCom :ERROR:TransceiveProcess Transceive send failed, going to recovery!
smCom :ERROR:phNxpEseProto7816_Close TransceiveProcess failed
smCom :ERROR:Failed to close session
App   :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
smCom :ERROR:Failed writing data (nrWritten=-1).

smCom :ERROR: - Error in I2C Write.....
smCom :ERROR:phNxpEseProto7816_SendRawFrame Error phNxpEse_WriteFrame
smCom :ERROR:TransceiveProcess Transceive send failed, going to recovery!
smCom :ERROR:phNxpEseProto7816_Open failed
smCom :ERROR: Failed to Open session
sss   :ERROR:SM_Connect Failed. Status 7012
App   :ERROR:sss_session_open failed
App   :ERROR:Session Open Failed
App   :INFO :Destroyed mutex
error: PKCS11 function C_OpenSession failed: rv = CKR_GENERAL_ERROR (0x5)
Aborting.
ssse-flw: EmbSe_Destroy(): Entry

 

 

Now here it is where it gets interesting: comparing the straces of seTool and any of the commands that do not work, reveal one difference in the i2c connect sequence: `write(3, "Z\300\0\377\374", 5)` call fails in the latter case, while works for the former. Here come the two strace snippets: 

 

# seTools, (works):
18659 10:12:30.522584 openat(AT_FDCWD, "/dev/i2c-1", O_RDWR) = 3 <0.000063>
18659 10:12:30.522760 ioctl(3, _IOC(_IOC_NONE, 0x7, 0x3, 0), 0x48) = 0 <0.000047>
18659 10:12:30.522928 ioctl(3, _IOC(_IOC_NONE, 0x7, 0x8, 0), 0) = 0 <0.000032>
18659 10:12:30.523316 ioctl(3, _IOC(_IOC_NONE, 0x7, 0x5, 0), 0x7ee2187c) = 0 <0.000037>
18659 10:12:30.523509 nanosleep({tv_sec=0, tv_nsec=5000000}, NULL) = 0 <0.007258>
18659 10:12:30.531005 read(3, 0x7ee2161c, 260) = -1 EREMOTEIO (Remote I/O error) <0.000179>
18659 10:12:30.531346 nanosleep({tv_sec=0, tv_nsec=1000000}, NULL) = 0 <0.001129>
18659 10:12:30.532644 write(3, "Z\300\0\377\374", 5) = 5 <0.000640>
# pkcs11-tool (does not work)
18684 10:13:47.901991 openat(AT_FDCWD, "/dev/i2c-1", O_RDWR) = 3 <0.000071>
18684 10:13:47.902200 ioctl(3, _IOC(_IOC_NONE, 0x7, 0x3, 0), 0x48) = 0 <0.000041>
18684 10:13:47.902344 ioctl(3, _IOC(_IOC_NONE, 0x7, 0x8, 0), 0) = 0 <0.000034>
18684 10:13:47.902473 ioctl(3, _IOC(_IOC_NONE, 0x7, 0x5, 0), 0x7ecf65c4) = 0 <0.000034>
18684 10:13:47.902662 nanosleep({tv_sec=0, tv_nsec=5000000}, NULL) = 0 <0.005108>
18684 10:13:47.907892 read(3, 0x7ecf6364, 260) = -1 EREMOTEIO (Remote I/O error) <0.000176>
18684 10:13:47.908185 nanosleep({tv_sec=0, tv_nsec=1000000}, NULL) = 0 <0.001099>
18684 10:13:47.909392 write(3, "Z\300\0\377\374", 5) = -1 EREMOTEIO (Remote I/O error) <0.000169>

 

Every other attempt with:

* the python scripts (/home/se050_middleware/simw-top/sss/plugin/openssl/scripts) `export EX_SSS_BOOT_SSS_PORT=/dev/i2c-1; export OPENSSL_CONF=/etc/ssl/nxp_openssl.cnf; python3 openssl_provisionEC.py --key_type prime256v1`

* the openssl command `openssl req -new -x509 -subj "/CN=Units" -engine e4sss -keyform engine -key 'pkcs11:id=xxxx;type=private' -out cert.pem` (with openssl configured with /usr/local/lib/libsss_engine.so),

* ssscli

fails in the same way.

 any help would be greatly appreciated! It is crucial from the business perspective for me to get it working.

 

best regards,

peter

 

0 Kudos
Reply
4 Replies

2,921 Views
ayoubzaki
Contributor I

The pkcs11 example from SE050-PLUG-TRUST-MW/simw-top/doc/plugins/pkcs11.html is NOT working (Version 04.02.00):

I have built the middleware using the following cmake options :

 

EXTRA_OECMAKE = " -DPTMW_Host=iMXLinux -DPTMW_HostCrypto=OPENSSL -DPTMW_SMCOM=T1oI2C \
-DPTMW_SE05X_Auth=None -DPTMW_SE05X_Ver=03_XX -DPTMW_Applet=SE05X_C \
-DCMAKE_BUILD_TYPE=Release -DSSS_HAVE_HOSTCRYPTO_MBEDTLS=ON -DRTOS_Default=ON"

 

# export EX_SSS_BOOT_SSS_PORT=/dev/i2c-1

# se05x_GetInfo
App :INFO :PlugAndTrust_v04.02.00_20220524
App :INFO :Running se05x_GetInfo
App :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
App :WARN :No SemsLite Applet Available.
App :INFO :Running se05x_GetInfo
App :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!
App :WARN :#####################################################
App :INFO :uid (Len=18)
04 00 50 01 12 C6 95 52 78 CE 6D 04 48 5F EA BA
6A 80
App :WARN :#####################################################
App :INFO :Applet Major = 3
App :INFO :Applet Minor = 1
App :INFO :Applet patch = 1
App :INFO :AppletConfig = 479A
App :INFO :With ECDSA_ECDH_ECDHE
App :INFO :WithOut EDDSA
App :INFO :With DH_MONT
App :INFO :With HMAC
App :INFO :WithOut RSA_PLAIN
App :INFO :WithOut RSA_CRT
App :INFO :With AES
App :INFO :With DES
App :INFO :With PBKDF
App :INFO :With TLS
App :INFO :WithOut MIFARE
App :INFO :WithOut I2CM
App :INFO :Internal = 010B
App :WARN :#####################################################
App :INFO :Tag value - proprietary data 0xFE = 0xFE
App :INFO :Length of following data 0x45 = 0x45
App :INFO :Tag card identification data (Len=2)
DF 28
App :INFO :Length of card identification data = 0x42
App :INFO :Tag configuration ID (Must be 0x01) = 0x01
App :INFO :Configuration ID (Len=12)
00 03 A2 05 5A 4B 63 E5 51 8D 0C C4
App :INFO :OEF ID (Len=2)
A2 05
App :INFO :Tag patch ID (Must be 0x02) = 0x02
App :INFO :Patch ID (Len=8)
00 00 00 00 00 00 00 01
App :INFO :Tag platform build ID1 (Must be 0x03) = 0x03
App :INFO :Platform build ID (Len=24)
4A 33 52 33 35 31 30 32 31 45 45 45 30 34 30 30
BC 03 04 79 33 8D 18 10
App :INFO :JCOP Platform ID = J3R351021EEE0400
App :INFO :Tag FIPS mode (Must be 0x05) = 0x05
App :INFO :FIPS mode var = 0x00
App :INFO :Tag pre-perso state (Must be 0x07) = 0x07
App :INFO :Bit mask of pre-perso state var = 0x00
App :INFO :Tag ROM ID (Must be 0x08) = 0x08
App :INFO :ROM ID (Len=8)
2E 5A D8 84 09 C9 BA DB
App :INFO :Status Word (SW) (Len=2)
90 00
App :INFO :se05x_GetInfoPlainApplet Example Success !!!...
App :WARN :#####################################################
App :INFO :cplc_data.IC_fabricator (Len=2)
47 90
App :INFO :cplc_data.IC_type1 (Len=2)
D3 21
App :INFO :cplc_data.Operating_system_identifier (Len=2)
47 00
App :INFO :cplc_data.Operating_system_release_date (Len=2)
00 00
App :INFO :cplc_data.Operating_system_release_level (Len=2)
00 00
App :INFO :cplc_data.IC_fabrication_date (Len=2)
00 23
App :INFO :cplc_data.IC_Serial_number (Len=4)
15 87 31 99
App :INFO :cplc_data.IC_Batch_identifier (Len=2)
44 17
App :INFO :cplc_data.IC_module_fabricator (Len=2)
00 00
App :INFO :cplc_data.IC_module_packaging_date (Len=2)
00 00
App :INFO :cplc_data.ICC_manufacturer (Len=2)
00 00
App :INFO :cplc_data.IC_embedding_date (Len=2)
00 00
App :INFO :cplc_data.IC_OS_initializer (Len=2)
08 48
App :INFO :cplc_data.IC_OS_initialization_date (Len=2)
5F 35
App :INFO :cplc_data.IC_OS_initialization_equipment (Len=4)
38 37 33 31
App :INFO :cplc_data.IC_personalizer (Len=2)
00 00
App :INFO :cplc_data.IC_personalization_date (Len=2)
00 00
App :INFO :cplc_data.IC_personalization_equipment_ID (Len=4)
00 00 00 00
App :INFO :cplc_data.SW (Len=2)
90 00
App :INFO :ex_sss Finished

 

ls -l /usr/lib/libsss_pkcs11.so
-rwxr-xr-x 1 root root 559808 Jul 18 08:19 /usr/lib/libsss_pkcs11.so

 

# pkcs11-tool --module /usr/lib/libsss_pkcs11.so --keypairgen --key-type rsa:1024 --label "sss:11223344"
Using slot 0 with a present token (0x1)
smCom :WARN :Invalid conn_ctx
App :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!
sss :WARN :nxEnsure:'ret == SM_OK' failed. At Line:6971 Function:sss_se05x_TXn
sss :WARN :nxEnsure:'status == SM_OK' failed. At Line:3578 Function:sss_se05x_key_store_generate_key
error: PKCS11 function C_GenerateKeyPair failed: rv = CKR_FUNCTION_FAILED (0x6)
Aborting.


what am I missing ?

0 Kudos
Reply

2,919 Views
ayoubzaki
Contributor I

The pkcs11 example from SE050-PLUG-TRUST-MW/simw-top/doc/plugins/pkcs11.html is NOT working (Version 04.02.00):

I have built the middleware using the following cmake options :

 

EXTRA_OECMAKE = " -DPTMW_Host=iMXLinux -DPTMW_HostCrypto=OPENSSL -DPTMW_SMCOM=T1oI2C \
-DPTMW_SE05X_Auth=None -DPTMW_SE05X_Ver=03_XX -DPTMW_Applet=SE05X_C \
-DCMAKE_BUILD_TYPE=Release -DSSS_HAVE_HOSTCRYPTO_MBEDTLS=ON -DRTOS_Default=ON"

 

# export EX_SSS_BOOT_SSS_PORT=/dev/i2c-1

# se05x_GetInfo
App :INFO :PlugAndTrust_v04.02.00_20220524
App :INFO :Running se05x_GetInfo
App :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
App :WARN :No SemsLite Applet Available.
App :INFO :Running se05x_GetInfo
App :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!
App :WARN :#####################################################
App :INFO :uid (Len=18)
04 00 50 01 12 C6 95 52 78 CE 6D 04 48 5F EA BA
6A 80
App :WARN :#####################################################
App :INFO :Applet Major = 3
App :INFO :Applet Minor = 1
App :INFO :Applet patch = 1
App :INFO :AppletConfig = 479A
App :INFO :With ECDSA_ECDH_ECDHE
App :INFO :WithOut EDDSA
App :INFO :With DH_MONT
App :INFO :With HMAC
App :INFO :WithOut RSA_PLAIN
App :INFO :WithOut RSA_CRT
App :INFO :With AES
App :INFO :With DES
App :INFO :With PBKDF
App :INFO :With TLS
App :INFO :WithOut MIFARE
App :INFO :WithOut I2CM
App :INFO :Internal = 010B
App :WARN :#####################################################
App :INFO :Tag value - proprietary data 0xFE = 0xFE
App :INFO :Length of following data 0x45 = 0x45
App :INFO :Tag card identification data (Len=2)
DF 28
App :INFO :Length of card identification data = 0x42
App :INFO :Tag configuration ID (Must be 0x01) = 0x01
App :INFO :Configuration ID (Len=12)
00 03 A2 05 5A 4B 63 E5 51 8D 0C C4
App :INFO :OEF ID (Len=2)
A2 05
App :INFO :Tag patch ID (Must be 0x02) = 0x02
App :INFO :Patch ID (Len=8)
00 00 00 00 00 00 00 01
App :INFO :Tag platform build ID1 (Must be 0x03) = 0x03
App :INFO :Platform build ID (Len=24)
4A 33 52 33 35 31 30 32 31 45 45 45 30 34 30 30
BC 03 04 79 33 8D 18 10
App :INFO :JCOP Platform ID = J3R351021EEE0400
App :INFO :Tag FIPS mode (Must be 0x05) = 0x05
App :INFO :FIPS mode var = 0x00
App :INFO :Tag pre-perso state (Must be 0x07) = 0x07
App :INFO :Bit mask of pre-perso state var = 0x00
App :INFO :Tag ROM ID (Must be 0x08) = 0x08
App :INFO :ROM ID (Len=8)
2E 5A D8 84 09 C9 BA DB
App :INFO :Status Word (SW) (Len=2)
90 00
App :INFO :se05x_GetInfoPlainApplet Example Success !!!...
App :WARN :#####################################################
App :INFO :cplc_data.IC_fabricator (Len=2)
47 90
App :INFO :cplc_data.IC_type1 (Len=2)
D3 21
App :INFO :cplc_data.Operating_system_identifier (Len=2)
47 00
App :INFO :cplc_data.Operating_system_release_date (Len=2)
00 00
App :INFO :cplc_data.Operating_system_release_level (Len=2)
00 00
App :INFO :cplc_data.IC_fabrication_date (Len=2)
00 23
App :INFO :cplc_data.IC_Serial_number (Len=4)
15 87 31 99
App :INFO :cplc_data.IC_Batch_identifier (Len=2)
44 17
App :INFO :cplc_data.IC_module_fabricator (Len=2)
00 00
App :INFO :cplc_data.IC_module_packaging_date (Len=2)
00 00
App :INFO :cplc_data.ICC_manufacturer (Len=2)
00 00
App :INFO :cplc_data.IC_embedding_date (Len=2)
00 00
App :INFO :cplc_data.IC_OS_initializer (Len=2)
08 48
App :INFO :cplc_data.IC_OS_initialization_date (Len=2)
5F 35
App :INFO :cplc_data.IC_OS_initialization_equipment (Len=4)
38 37 33 31
App :INFO :cplc_data.IC_personalizer (Len=2)
00 00
App :INFO :cplc_data.IC_personalization_date (Len=2)
00 00
App :INFO :cplc_data.IC_personalization_equipment_ID (Len=4)
00 00 00 00
App :INFO :cplc_data.SW (Len=2)
90 00
App :INFO :ex_sss Finished

 

ls -l /usr/lib/libsss_pkcs11.so
-rwxr-xr-x 1 root root 559808 Jul 18 08:19 /usr/lib/libsss_pkcs11.so

 

# pkcs11-tool --module /usr/lib/libsss_pkcs11.so --keypairgen --key-type rsa:1024 --label "sss:11223344"
Using slot 0 with a present token (0x1)
smCom :WARN :Invalid conn_ctx
App :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss :INFO :atr (Len=35)
00 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 08
01 00 00 00 00 64 00 00 0A 4A 43 4F 50 34 20 41
54 50 4F
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!
sss :WARN :nxEnsure:'ret == SM_OK' failed. At Line:6971 Function:sss_se05x_TXn
sss :WARN :nxEnsure:'status == SM_OK' failed. At Line:3578 Function:sss_se05x_key_store_generate_key
error: PKCS11 function C_GenerateKeyPair failed: rv = CKR_FUNCTION_FAILED (0x6)
Aborting.


what am I missing ?

Tags (1)
0 Kudos
Reply

4,070 Views
peter_nt
Contributor I

an update: when I have the gdb running:

root@raspberrypi:/home/se050_middleware/simw-top/demos/se05x/seTool# ps axuw | grep gdb
root     19894  0.3  4.6  53500 44184 pts/2    S+   13:33   0:06 gdb --args /home/se050_middleware/simw-top_build/raspbian_native_se050_t1oi2c/bin/seTool genECC 0x01010101 /dev/i2c-1

the pkcs11-tool command works, (as well as the python scripts examples)

root@raspberrypi:/home/se050_middleware/simw-top/demos/se05x/seTool# pkcs11-tool --module $PKCS11_MODULE --keypairgen --key-type rsa:1024 --label "sss:20202020"
ssse-flw: EmbSe_Init(): Entry
App   :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss   :INFO :atr (Len=35)
      00 A0 00 00    03 96 04 03    E8 00 FE 02    0B 03 E8 08
      01 00 00 00    00 64 00 00    0A 4A 43 4F    50 34 20 41
      54 50 4F
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
ssse-flw: Version: 1.0.5
ssse-flw: EmbSe_Init(): Exit
ssse-flw: EmbSe_Finish(): Entry
ssse-flw: EmbSe_Finish(): Exit
Using slot 0 with a present token (0x1)
smCom :ERROR:phNxpEseProto7816_SendRawFrame Error phNxpEse_WriteFrame
smCom :ERROR:TransceiveProcess Transceive send failed, going to recovery!
smCom :ERROR:phNxpEseProto7816_Close TransceiveProcess failed
smCom :ERROR:Failed to close session
App   :INFO :Using PortName='/dev/i2c-1' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1)
sss   :INFO :atr (Len=35)
      00 A0 00 00    03 96 04 03    E8 00 FE 02    0B 03 E8 08
      01 00 00 00    00 64 00 00    0A 4A 43 4F    50 34 20 41
      54 50 4F
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
App   :INFO :Destroyed mutex
Key pair generated:
Private Key Object; RSA
  label:      sss:20202020
  ID:         20202020
  Usage:      decrypt, signApp   :WARN :Attribute required : 0xcf534301


Private Key Object; RSA
  label:      sss:20202020
  ID:         20202020
  Usage:      decrypt, signApp   :WARN :Attribute required : 0xcf534301


App   :INFO :Destroyted mutex
App   :INFO :SessionCount = 0
ssse-flw: EmbSe_Destroy(): Entry

the gdb is stopped at:

106	    if (ioctl(axSmDevice, I2C_FUNCS, &funcs) < 0)
(gdb) p funcs
$4 = 66
(gdb) bt
#0  axI2CInit (conn_ctx=0x7efff894, pDevName=0x7efffd3c "/dev/i2c-1")
    at /home/se050_middleware/simw-top/hostlib/hostLib/platform/linux/i2c_a7.c:106
0 Kudos
Reply

4,043 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @peter_nt ,

 

Did you build the PKCS#11 library as below:

PKCS build.png

Please kindly refer to "SE050-PLUG-TRUST-MW/simw-top/doc/plugins/pkcs11.html" for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply