EB Tresos config FS26's Watch Dog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB Tresos config FS26's Watch Dog

4,428 Views
shiqi_seventeen
Contributor III

Hello Team:

 I am using EB Tresos config FS26's Watching Dog,but I found some files  are not generated ,like : Wdg_43_fs26_cfg.h.

And it is necessary in my project ,because  I found it appear in demo project

shiqi_seventeen_0-1712450992111.png

shiqi_seventeen_1-1712451129320.png

 

So how can I solve it ? 

Thanks ! 

 

 

0 Kudos
Reply
8 Replies

4,408 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

I am not familiar with this  EB Tresos and the software, if you have any WD configuration produce issue or questions please let me know.

 

0 Kudos
Reply

4,384 Views
shiqi_seventeen
Contributor III

我发现在SBC_FS26下的MCAL 2.0.0版本:

shiqi_seventeen_0-1712546912868.png

有两个子模块:SBC_FS26与WDG_43_FS26

shiqi_seventeen_1-1712546980475.png

然后我在配置的时候,除了WDG_43_FS26模块可以配置窗口看门狗,发现在SBC_FS26模块中也可以配置窗口看门狗

那么我想请教两个问题

1.这两个模块中配置的看门狗 在软件配置和硬件配置上有什么不同?

2.第二个问题如图所示

shiqi_seventeen_2-1712547529519.png

 

0 Kudos
Reply

4,372 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个应该是MCU的团队写的程序,我这边只负责FS26,如果您有具体的FS26的问题比方说WD的问题可以帮助到您。

0 Kudos
Reply

4,356 Views
shiqi_seventeen
Contributor III

好的谢谢

那请问您这边知道如何进行SBC的喂狗吗?因为我这是我第一次接触SBC看门狗,但SBC提供的MCAL包里面没有提供相关看门狗例程。所以想问问您这边知道怎么去喂SBC的看门狗吗?是定时去改变token值,然后计算answers值,再通过SPI发送到SBC中吗?还是说怎么去刷新喂狗。感谢

0 Kudos
Reply

4,349 Views
guoweisun
NXP TechSupport
NXP TechSupport

你好:

首先要知道手上的FS26 是Challenger watchdog 还是Simple watchdog跟选择的part number有关系。

然后看datasheet page165 页,跟AN12995的第54页

0 Kudos
Reply

4,338 Views
shiqi_seventeen
Contributor III
我的是Challenger watchdog ;然后您这边有AN12995的文档吗,我手上只有一份FS26 3.0.0的datasheet
0 Kudos
Reply

4,336 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个文档是加密的要NDA,你可以登陆到页面下下载或者申请下载:

guoweisun_0-1712626023404.png

 

0 Kudos
Reply

4,282 Views
shiqi_seventeen
Contributor III

你好:
现在我请教一些关于LDT定时唤醒的问题:定时唤醒和休眠时长统计我单独已经开发并测试好了,现在就是项目中要求这两个功能同时实现。但我发现这两个功能,都是使用同一个函数入口Sbc_fs26_SetLDT()(写入的寄存器都是M_LDT_CTRL),且使用Sbc_fs26_SetLDT()函数要在SBC休眠之前调用,所以我的疑惑是如果同时开启这两个功能(定时唤醒和休眠时长统计),意味着得调用Sbc_fs26_SetLDT()函数两次,那么是不是第一次调用Sbc_fs26_SetLDT函数(写入数据到M_LDT_CTRL寄存器实现定时唤醒)会被第二次调用Sbc_fs26_SetLDT(写入数据到M_LDT_CTRL寄存器实现统计休眠时长计)刷新掉?

shiqi_seventeen_0-1712814999406.png

 

0 Kudos
Reply