Hey guys. I new to KIT 33816 board and I am using it to do the injection and control the pumping control valve. Now, I want to control the behavior of injection and pumping control valve in LABView since some feedback signals which are used to do a closed loop control come into the LABView. But here is problem, how can I run different single command or batch command automatically after I change the parameters in the configuration registers?
Best regards,
Shuai