Documentation for MPC5777C-516DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Documentation for MPC5777C-516DS

跳至解决方案
1,902 次查看
raul10
Contributor I

Where can I find the documentation for the evaluation board MPC5777C-516DS?

I bought this board, but there was no documentation included. I need especially the description of the jumper settings for generating the power supplies on board since I have no motherboard.

0 项奖励
1 解答
464 次查看
marco_sacchi
NXP Employee
NXP Employee

The documentation isn't available because the MCU hasn't been qualified.

Please find attached the schematics of the daughter board MPC5777-516DS. The board is configured by default to work with the motherboard, which is providing the power suplly.

In order to configure it to obtain the power supply from the regulator mounted on the MPC5777C-516DS the following modification to the jumpers default settings should be applied:

J2 -> 1-2    (5.0V_SR from the onboard switching regulator)

J3 -> 1-2    (3.3V_SR from the onboard switching regulator)

J22 -> 1-3 1.25V_SR connected the the 1.25V obtained from the on-bboard linear regulator.

These changes should be enough to run the daughter board of Cobra55 alone.

在原帖中查看解决方案

0 项奖励
1 回复
465 次查看
marco_sacchi
NXP Employee
NXP Employee

The documentation isn't available because the MCU hasn't been qualified.

Please find attached the schematics of the daughter board MPC5777-516DS. The board is configured by default to work with the motherboard, which is providing the power suplly.

In order to configure it to obtain the power supply from the regulator mounted on the MPC5777C-516DS the following modification to the jumpers default settings should be applied:

J2 -> 1-2    (5.0V_SR from the onboard switching regulator)

J3 -> 1-2    (3.3V_SR from the onboard switching regulator)

J22 -> 1-3 1.25V_SR connected the the 1.25V obtained from the on-bboard linear regulator.

These changes should be enough to run the daughter board of Cobra55 alone.

0 项奖励