Difference between the MPC860TZQ80D4 and the MPC860TVR80D4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between the MPC860TZQ80D4 and the MPC860TVR80D4

465 次查看
arakotomalala
Contributor I

I would like to know the difference between the MPC860TZQ80D4 and the MPC860TVR80D4.
Are they equivalent (Same Fit & Function, Pin-for-Pin Equivalent, ...)?

0 项奖励
1 回复

392 次查看
alexander_yakov
NXP Employee
NXP Employee

The difference between package suffix "ZQ" anf "VR" is in leaded package for "ZQ", whereas "VR" is lead-free RoHS compliant. There is no other difference, both devices are pin-compatible and functionally identical, have the same silicon inside. Note lead-free device require another soldering process, with higher temperature.

0 项奖励