Detect and get uID Mifare DesFire Ev3 card on IOS (swift).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Detect and get uID Mifare DesFire Ev3 card on IOS (swift).

1,127件の閲覧回数
congpt
Contributor I

Hi all!
Can someone help me? I have several Mifare DesFire Ev3 cards. I am trying to detect and get the UID of a card on my IOS app but it fails.

Here's what I'm doing:

@available(iOS 13, *)

    func beginScanning() {

        let sessiont = NFCTagReaderSession(pollingOption: .iso14443, delegate: self)

        sessiont.alertMessage = "vID.startSS.holdWn".localizableString()

        sessiont.begin()

    }

 

    @available(iOS 13, *)

    func tagReaderSession(_ session: NFCTagReaderSession, didDetect tags: [NFCTag]) {

        LogVM.log("Read tag:")

        if case let NFCTag.miFare(tag) = tags.first! {

            LogVM.log("=> Is tag mife:")

            LogVM.log(tag.identifier.hexEncodedString(options: .upperCase))

        }

    }

When I touch the ev3 tag it doesn't even jump to the "didDetect tags" function and "LogVM.log("Read tag:")".

The code works great with my ev2 tag, it easily detects the tag and gets the uID on the ev2 tag.

How can I detect Ev3 tags?
Note: I tried detecting it on NXP's "Tag Info" application. It detected that it was indeed a Mifare DesFire Ev3 card.

タグ(5)
0 件の賞賛
1 返信

1,117件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @congpt ,

 

We are just IC supplier, only can provide documentation regarding Mifare DESFire EV3, for iOS development issue, you have to ask for help from Apple.

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛