Designing for high frequency of MRFE6VP100HR5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Designing for high frequency of MRFE6VP100HR5

495 Views
surajkantsingh0
Contributor I

I want to design high frequency schematic for MRFE6VP100HR5 IC for high power upto 100W in the frequency range of 500-1000 MHz. Can you assist me regarding the any relevant document for designing or Simulation software which can help me regarding the same?

0 Kudos
1 Reply

428 Views
LPP
NXP Employee
NXP Employee

NXP offers MRFE6VP100H reference design for 400-1000MHz frequency range. You can order this board through our authorized distributors as fully assembled and tested circuit or as a kit that includes PCB samples and all the components required. I sent the documentation pack to your mail.


Have a great day,
Pavel
NXP TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos