DSP 56f8367 clock problem ?!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP 56f8367 clock problem ?!

ソリューションへジャンプ
2,774件の閲覧回数
TroyCorser
Contributor III
Hi all,
I have this problem:
I program my DSP with USB TAP (ldm Internal memory: pROM-to-xRAM) and all work properly, but when I reset the DSP by a Power off something happen.
When I power on the DSP it works but it seem works with a different time extension like if the clock period is altered.
To explain better:
I introduce a delay, of 1 second, in a simple cycle.
It works with this delay time till I switch off the power.
When I switch on the power the time delay, that was of 1 second before, now take about 15 seconds... how could it be?
I'm not using the procesor expert, but simple C code wrote all by myself.
I think it's not a hardware problem because I create a similar procedure with processor expert and it works properly also after a power on reset.
If someone know any possible reason / solution ...
ラベル(1)
  • DSC

タグ(2)
0 件の賞賛
返信
1 解決策
1,612件の閲覧回数
TroyCorser
Contributor III
I solved the problem.
 
There was a multyple memory configuration in the file 56F83x_init.asm
 
pROM-to-xRAM utility and also xRom-to-xRam

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,613件の閲覧回数
TroyCorser
Contributor III
I solved the problem.
 
There was a multyple memory configuration in the file 56F83x_init.asm
 
pROM-to-xRAM utility and also xRom-to-xRam
0 件の賞賛
返信