Custom Firmware image creation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom Firmware image creation

Jump to solution
796 Views
Ghouse
Contributor V

Hi, iam using LS1046ardb in a custom card, i want to change the rcw file and build the firmware image with the modified rcw file.

please provide the complete process for generating custom firmware image using modified .rcw file.

Although flex-builder -c rcw -m ls1046ardb can be used to make the "bl2_qspi.pbl",  i want to know if there a procedure to generate the firmware image using .rcw or bl2_qspi.pbl..

0 Kudos
Reply
1 Solution
775 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to file configs/board/ls1046ardb/manifest, rcw_1800_qspiboot.bin is used to generate atf/firmware image.

rcw_qspi="firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.bin"

1. Please execute the following command.

$ flex-builder -c rcw -m ls1046ardb

2. Please modify RCW file components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.rcw for your custom board.

3. Rebuild rcw and atf.

$ flex-builder -c rcw -m ls1046ardb

$ flex-builder -c atf -m ls1046ardb -b qspi

4. $ flex-builder -i mkfw -m ls1046ardb -b qspi

View solution in original post

0 Kudos
Reply
1 Reply
776 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to file configs/board/ls1046ardb/manifest, rcw_1800_qspiboot.bin is used to generate atf/firmware image.

rcw_qspi="firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.bin"

1. Please execute the following command.

$ flex-builder -c rcw -m ls1046ardb

2. Please modify RCW file components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.rcw for your custom board.

3. Rebuild rcw and atf.

$ flex-builder -c rcw -m ls1046ardb

$ flex-builder -c atf -m ls1046ardb -b qspi

4. $ flex-builder -i mkfw -m ls1046ardb -b qspi

0 Kudos
Reply