Controlling MC33772C via direct SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Controlling MC33772C via direct SPI

1,087 Views
hbsantos
Contributor II

I need to control the mc33772c via the s32k344 SPI, but I'm using the Bms_common SDK library with mc33665A and mc33775a. is it possible to create a second instance of bms_common to control the mc33772c? Or is there another possibility of configuration via direct SPI communication with the mc33772c?

 

hbsantos_0-1706016650998.png

Tags (4)
0 Kudos
Reply
2 Replies

1,060 Views
guoweisun
NXP TechSupport
NXP TechSupport

If you don't need TPL communication you can directly build the SPI communication between MC3377X and MCU:

guoweisun_0-1706233892220.png

 

0 Kudos
Reply

1,019 Views
hbsantos
Contributor II

Ok, but I would like to use the BMS SDK, is it possible? Because the MC33772C driver is not compatible with S32K3 micrcontrollers.

Tags (2)
0 Kudos
Reply