CodeWarrior USB TAP can not connect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior USB TAP can not connect

1,268 次查看
yqypower
Contributor I

When I use the CodeWarrior USB TAP to connect MCP8309,it
always returns "Please check your JTAG clock speed",so I
change another CodeWarrior USB TAP,it works well!

My trouble
is How to  repair it?

0 项奖励
回复
1 回复

1,263 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Did you use CodeWarrior 10.5.1 or CodeWarrior 8.8?

Is the problem USB TAP a CodeWarrior TAP which integrates both USB and Ethernet ports?

Is there valid RCW on MPC8309 custom board?

Please open CCS console from Start->Freescale CodeWarrior->CodeWarrior Connection Server and type the following commands to do more verification.

(bin) 3 % delete all
(bin) 4 % config cc cwtap
(bin) 5 % show cc
CodeWarrior TAP executable differs from local file.
CodeWarrior TAP Boot Loader version 1.0.1
CodeWarrior TAP OS version 1.0.1
Sending code to CodeWarrior TAP.........done
Running package script
0: CodeWarrior TAP (cwtap) CC software ver. {0.0}
(bin) 6 % source IDcode.tcl

Scanning for available TAPs connected via USB.....


++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
+
+ Available Remote Connections
+
+ 1 - CodeWarriorTAP - 00:04:9f:02:f1:ea
+ 2 - CodeWarriorTAP - <Specify IP Address>
+ 3 - EthernetTAP - <Specify IP Address>
+ 4 - GigabitTAP - <Specify IP Address>
+
+ x - Exit Script without Changes
+
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++

Specify connection:
1

Configuring TAP Interface....

Configured Connection: cwtap : 00:04:9f:02:f1:ea

 

 

0 项奖励
回复