Clean-in-box MPC8315E-RDB for sale

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clean-in-box MPC8315E-RDB for sale

3,180 Views
RabbitHoleComp
Contributor II
I have an essentially unused MPC8315E-RDB devkit/reference platform in the original freescale box, with all software, cables, and international power adapters. I'm located in California but am happy to ship anywhere in the world if you're willing to cover actual shipping costs. I'm hoping to get $275+shipping for i, but no reasonable offer will be refused. I'm only getting rid of it because I'm not using it. The box happily boots up into Linux off its SATA drive. Please contact me privately via e-mail to aperez _#at#_ inertial #dawt# biz or reply to the post here
0 Kudos
Reply
5 Replies

2,322 Views
TMM
Contributor II

This is a bit of a long shot, but do you still have this thing for sale? I've been looking for one!

0 Kudos
Reply

2,818 Views
rmbvector
Contributor I

I'm interested in purchasing a MPC8315E-RDB.  Do you know if there is an external pod or emulator that is needed to connect to this dev board? i can't seem to find much detailed info on the connection method from the host PC to this board. Also using a windows based host PC. Have you already used this board?

 

thanks

Rob

 

0 Kudos
Reply

2,818 Views
RabbitHoleComp
Contributor II

It's still available. Where are you located? The board comes with u-boot installed, and is very easy to use. 

0 Kudos
Reply

2,818 Views
rmbvector
Contributor I

located in Rhode Island USA 02818

do you use the CW USB TAP to connet to the board? 

0 Kudos
Reply

2,818 Views
RabbitHoleComp
Contributor II

I have not used the CW USB TAP, but I am sure it would work fine.

0 Kudos
Reply