Capturing an iamge and Recording a video from Camera and Encoding Camera's O/P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capturing an iamge and Recording a video from Camera and Encoding Camera's O/P

Jump to solution
5,649 Views
nikhil29
Contributor III

Hello NXP

I'm working on a camera related project [ Using C Programming Only ] for that i need your help.

1]  to capture an image and record a video and then encode the same.

2]  after that i need to downscale that image and send to TV [ Host ].

 

So, to execute the above things could you please share some methods / tools / libraries / techniques to do the same.

 

Q1 : If i could use GStreamer, then i want to know the difference between how to capture / record    and  encode using GStreamer plugins  ??  [ Difference between record / capture and encode via GStreamer ]

Q2 : and for downscaling could i use OpenCV [ for C programming only ]  ?? 

If yes, then send me PDF / tools / libraries / methods realted to OpenCV

  

Thanks

Nikhil

0 Kudos
1 Solution
5,629 Views
igorpadykov
NXP Employee
NXP Employee

Hi nikhil29

 

what processor used in the case. One can start with Chapter 6 Video

i.MX Linux Reference Manual​

Chapter 10 Unit Tests

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.24_2.1.0

Gstreamer examples in sect.7.3 Multimedia use cases i.MX Linux User’s Guide​

 

Best regards
igor

View solution in original post

0 Kudos
7 Replies
1,019 Views
tracyberge
Contributor I

No matter how long you have played, you will still not be able to accurately estimate the altitude of each takeoff. Therefore, any water pipe will be an extremely difficult challenge.  Flappy Bird

0 Kudos
1,141 Views
dalesmith657
Contributor I

Dark Dale is a Digital Marketer and blogger who ensures that a consistent important message is delivered to the user. He is detail-oriented and talented, allowing him to incorporate his digital & blogging skills with his vision to identify user needs and provide the best information to his readers. <a href=https://www.gotoassignmenthelp.com/blog/highly-effective-assignment-help-services-for-students/

0 Kudos
1,400 Views
Root76
Contributor I

Thanks for one marvelous posting! I enjoyed reading it; you are a great author.I will make sure to bookmark your blog and may come back someday. I want to encourage that you continue your great posts, have a nice weekend!

Disneyplus.com/begin

Disneyplus.com/start

0 Kudos
5,630 Views
igorpadykov
NXP Employee
NXP Employee

Hi nikhil29

 

what processor used in the case. One can start with Chapter 6 Video

i.MX Linux Reference Manual​

Chapter 10 Unit Tests

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.24_2.1.0

Gstreamer examples in sect.7.3 Multimedia use cases i.MX Linux User’s Guide​

 

Best regards
igor

0 Kudos
5,595 Views
nikhil29
Contributor III

Thanks igor for your time

I'm using i.MX 8M Plus as a processor.

1)  could you please ellaborate diff. between record/capture and encoding via GStreamer

2)  what about OpneCV  ??

 

Thanks

nikhil

0 Kudos
5,587 Views
igorpadykov
NXP Employee
NXP Employee

Hi nikhil29

 

that processor is not supported yet, it is "Preproduction" part.

It will be supported after public launch.

 

 

1.jpg

 

Best regards
igor

0 Kudos
5,580 Views
nikhil29
Contributor III

Ok igor, thankuu for your time

 

Thanks

Nikhil

0 Kudos