Hello everyone,
I am using some SC16IS750 via I2C protocol. The SC16IS750 is addressed by using A1 and A0 pins as shown below. However, I can only use 4 cases (VDD-VDD, VDD-VSS, VSS-VDD, VSS-VSS). When one of the SC16IS750 that has A1 or A0 pin connected to SCL/SDA, then it cannot detect that address and also affact other SC16IS750.
So, how to fix this problem ?
Thank you for you consideration !
I have a similar issue.
For many years we use the TSSOP version, and all is fine.
A0 is connected directly to the SCL line. It works like a charm, no problems, many thousand units.
But now, I migrated to the HVQFN version and the I2C address is not correct, according the datasheet.
It is working on a different I2C adress than axpected.
The recommendation is the 10 Ohm resistor is not mentioned in the datasheet. Does this work? why?
Can you help me?