Can we externally flash in program ROM of PN7150 ? How to do so ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we externally flash in program ROM of PN7150 ? How to do so ?

448 Views
JagirMehta
Contributor II

Hello, I want to do some customization in PN7150 using its code memory. Please let me is it possible or not & If so then how to do it, Because I found there are only I2C interfaces available to be connected to the Device Host.

Labels (1)
Tags (1)
0 Kudos
1 Reply

427 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

That is not possible. The PN7150 is a NFC controller with integrated firmware. This IC is fully user controllable by the firmware interface, which cannot be changed.

 

Regards,

Ricardo

0 Kudos