Can't detect/discover type B (iso-14443 B) card using PN7150

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't detect/discover type B (iso-14443 B) card using PN7150

1,472 Views
iwannugraha
Contributor III

Hi,

Currently i'm using PN7150 with android board.
The NFC reader (PN7150) can be used to read type A cards, but cannot detect type B cards at all.

Below is the PCB antenna that I use :

NFC AntennaNFC Antenna

 

Antenna dimensionAntenna dimension

The following is a schematic for the antenna matching circuit:

matching Circuit Schematicmatching Circuit Schematic

I got the antenna matching values from the calculation results from the Antenna Calculator.

Antenna CalculatorAntenna Calculator

I did the tuning process for the values C0, C1, and C2 and used the RFSim99 application. Below are the simulation results on the RFSim99 application:

 

RFSim99 schematicRFSim99 schematicSmith chart simulation results from RFSim99:

RFSim99 Smith ChartRFSim99 Smith Chart

Below is the signal shape (Smith chart) of the measurement results on the PCB board using Nano VNA.

Measure the signal using nano vnaMeasure the signal using nano vna

 

actual signal shape using nanovnaactual signal shape using nanovna

 

Please help me!!

 

 

 

Labels (1)
  • RF

0 Kudos
Reply
2 Replies

1,377 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

The matching looks good. Need more information to check it.

 

Regards

Daniel

0 Kudos
Reply

1,363 Views
iwannugraha
Contributor III

Hi @danielchen ,

 

What you need?

 

Best Regards,

 

iwan

0 Kudos
Reply