Can sja1105 set a port to join all VLANs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can sja1105 set a port to join all VLANs

997 Views
liurunze
Contributor I

All types of VLANs are added, such as VLAN based on MAC address, not limited to VLAN divided by port

Tags (1)
0 Kudos
Reply
1 Reply

958 Views
bpe
NXP Employee
NXP Employee

SJA1105 can assign a VLAN tag based only on the ingress port. VLAN membership
is defined in VMEMB_PORT of VLAN Lookup table entry. If you wish all ports to
be members of a certain VLAN, you have to set the corresponding bit of VMEMB_PORT
in all VLAN Lookup table entries. See SJA1105TEL User Manual, Sections 4.2.8
and 4.2.10.


Have a great day,
Platon


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply