Can TJA1052iT meet the standard: GB/T 21437.3-2012(ISO 7637-3)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can TJA1052iT meet the standard: GB/T 21437.3-2012(ISO 7637-3)?

608 Views
yangmingsong
Contributor II

Recently, the end customer has proposed the requirement of electrical transient conduction immunity along the signal line / control line.

The question:Can the TJA1052iT  meet the Standard: Test in accordance with GB / T 21437.3-2012 (ISO 7637-3)?

1.png

Meet Class III requirements: The device or system can perform all its pre-designed functions during and after the harassment.

Schematic diagram:

2.jpg

0 Kudos
2 Replies

551 Views
guoweisun
NXP TechSupport
NXP TechSupport

可以满足的这个测试规则。

稍等我给你一个EMC测试的报告供参考通过邮件的方式

0 Kudos

551 Views
yangmingsong
Contributor II

Hi G.w.Sun

I have received the file, thank you for your support!

Best regards                       

Field Application Enginner – Mingsong Yang

0 Kudos