Can TJA1040 work normally at - 43 ℃?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can TJA1040 work normally at - 43 ℃?

867件の閲覧回数
zhangcope
Contributor I
Hello, can TJA1040 work normally at - 43 ℃?
タグ(1)
0 件の賞賛
返信
2 返答(返信)

667件の閲覧回数
vinythambi
Contributor I

Do we need impedance control for CAN bus traces? if yes, what is the value?

0 件の賞賛
返信

831件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Cope,

I have contacted an IVN team with your question. For the answer please see the description.

DESCRIPTION

TJA1040 is only guaranteed to work until Tj=-400C. Whether that allows -430C ambient to be used, really depends on the self-heating of TJA1043, in turn fully determined by the loading/duty cycle of the application. So customer has to detemine P for their application, nothing we can do.

 

Anyway, if it really depends on that, it means customer is really working at the edge, and will likely have problems guaranteeing with TJA1043 Tj=-400C.

With Best Regards,

Jozef

0 件の賞賛
返信