We are using CLRC663 in our project and load protocol function is working fine but the problem is in REQA is not responding. we followed all the instruction given in AN12657 document and also tried without Library examples but none of them is working. we observed that the REQA is getting transmitted successfully but after that we are neither receiving Rx interrupt, data, error. Please find below the REQA code. Can somebody help us to fix this issue or let us know if we are missing anything in the code.
uint8_t Load_Protocol_14443()
{
uint8_t errorRegister1;
write_reg(CLRC663_REG_COMMAND, CLRC663_CMD_IDLE);
write_reg(CLRC663_REG_FIFOCONTROL, 0xB0);
write_reg(CLRC663_REG_FIFODATA, 0x00);
write_reg(CLRC663_REG_FIFODATA, 0x00);
write_reg(CLRC663_REG_COMMAND, CLRC663_CMD_LOADPROTOCOL);
errorRegister1 = read_reg(CLRC663_REG_ERROR);
/* Checks if an Error has occurred*/
if (errorRegister1 != 0)
{
write_reg(CLRC663_REG_DRVMOD, 0x86);
return false;
}
return true;
}
uint8_t send_REQA()
{
write_reg(CLRC663_REG_COMMAND, CLRC663_CMD_IDLE);
write_reg(CLRC663_REG_FIFOCONTROL, 0xB0);
write_reg(CLRC663_REG_TXDATANUM, 7 | CLRC663_TXDATANUM_DATAEN);
write_reg(CLRC663_REG_TXCRCPRESET, CLRC663_RECOM_14443A_CRC | CLRC663_CRC_OFF);
write_reg(CLRC663_REG_RXCRCCON, CLRC663_RECOM_14443A_CRC | CLRC663_CRC_OFF);
write_reg(CLRC663_REG_RXBITCTRL, 0);
write_reg(CLRC663_REG_IRQ0, 0x7F);
write_reg(CLRC663_REG_IRQ1, 0x7F);
write_reg(CLRC663_REG_IRQ0EN, CLRC663_IRQ0EN_RX_IRQEN | CLRC663_IRQ0EN_ERR_IRQEN);// for global int
write_reg(CLRC663_REG_IRQ1EN, CLRC663_IRQ1EN_TIMER0_IRQEN); // only trigger on timer for irq1
uint8_t timer_for_timeout = 0;
CLRC663_timer_set_control(timer_for_timeout, CLRC663_TCONTROL_CLK_211KHZ | CLRC663_TCONTROL_START_TX_END);
// Frame waiting time: FWT = (256 x 16/fc) x 2 FWI
// FWI defaults to four... so that would mean wait for a maximum of ~ 5ms
CLRC663_timer_set_reload(timer_for_timeout, 1000); // 1000 ticks of 5 usec is 5 ms.
CLRC663_timer_set_value(timer_for_timeout, 1000);
write_reg(CLRC663_REG_COMMAND, CLRC663_CMD_IDLE);
write_reg(CLRC663_REG_FIFOCONTROL, 1<<4);
write_reg(CLRC663_REG_FIFODATA, 0x26);
write_reg(CLRC663_REG_COMMAND, CLRC663_CMD_TRANSCEIVE);
// write_reg(CLRC663_REG_IRQ1, 0x7F);
uint8_t irq1_value = 0;
while (!(irq1_value & (1 << timer_for_timeout)))
{
irq1_value =read_reg(CLRC663_REG_IRQ1);
if (irq1_value & 0x40)
{ // either ERR_IRQ or RX_IRQ
break; // stop polling irq1 and quit the timeout loop.
}
}
write_reg(CLRC663_REG_COMMAND, CLRC663_CMD_IDLE);
// if no Rx IRQ, or if there's an error somehow, return 0
uint8_t irq0 = read_reg(CLRC663_REG_IRQ0);
// if ((!(irq0 & 0x04)) || (irq0 & 0x02))
// {
// return 0;
// }
uint8_t rx_len = read_reg(CLRC663_REG_FIFOLENGTH);
uint8_t res, Register1,Register2;
__no_operation();
if (rx_len == 2) { // ATQA should answer with 2 bytes.
Register1 = read_reg(CLRC663_REG_FIFODATA);
Register2 = read_reg(CLRC663_REG_FIFODATA);
res = Register1;
res = Register2;
return res;
}
return 0;
}
void CLRC663_timer_set_control(uint8_t timer, uint8_t value)
{
write_reg(CLRC663_REG_T0CONTROL + (5 * timer), value);
}
void CLRC663_timer_set_reload(uint8_t timer, uint16_t value)
{
write_reg(CLRC663_REG_T0RELOADHI + (5 * timer), value >> 8);
write_reg(CLRC663_REG_T0RELOADLO + (5 * timer), value & 0xFF);
}
void CLRC663_timer_set_value(uint8_t timer, uint16_t value)
{
write_reg(CLRC663_REG_T0COUNTERVALHI + (5 * timer), value >> 8);
write_reg(CLRC663_REG_T0COUNTERVALLO + (5 * timer), value & 0xFF);
}
Hello @Pranav_Chilka
Thanks for contacting us and interested in the NXP products.
Based on your description, it's recommended that you check the following points:
1. whether the SPI or I2C driver works properly.
2. Please try to implement your project according to the logic steps of this example SW6693\RC663_Register_Example\Ex1_Simple_REQA.
3. You can use TagInfo (which is from NXP and running on Android/IOS device) to access your card or tag and confirm whether it's working properly.
To update this case, you may reply by email.
To provide confidential information or attachments, you may add that online.
Please login to our NXP technical support portal:
https://support.nxp.com/s/case/5002p00002s5WKwAAM
The portal allows access to the full details of the case, including the previous communication.
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Best regards,
Kelly
Technical Support
NXP Semiconductor