CAN tranceiver FMEA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN tranceiver FMEA

Jump to solution
3,459 Views
wenfengyao
Contributor II

In order to carry on the function safety analysis to the effect of each failure mode of CAN transceiver on function

Where can I find the FMEA file of the following devices?

TJA1043T

TJA1145T/FDJ

0 Kudos
Reply
1 Solution
3,437 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Wenfeng,

Those CAN transceivers are not ASIL devices and have not been developed according to ISO26262. FMEDA is hence not available. For failure modes we can offer the pin FMEA. For the TJA1043T on page 96 of the AH1014. And for the TJA1145T/FDJ on page 65 of the attached AH1309.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
3,438 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Wenfeng,

Those CAN transceivers are not ASIL devices and have not been developed according to ISO26262. FMEDA is hence not available. For failure modes we can offer the pin FMEA. For the TJA1043T on page 96 of the AH1014. And for the TJA1145T/FDJ on page 65 of the attached AH1309.

Best regards,

Tomas

0 Kudos
Reply