CAN Transceiver TJA1043T communication interrupted

cancel
Showing results for 
Search instead for 
Did you mean: 

CAN Transceiver TJA1043T communication interrupted

115 Views
Rio_Lee
Contributor I

The characteristics of CAN1 communication interruption are as follows: Under the monitoring of the upper computer monitoring interface, after power-on, if no instruction is sent, the state of CAN is always normal.It starts with instructions, works for a few times, and then after a few times, communication breaks down.

 

I observed the waveforms of pins VCC, EN, WAKE, ERR_N and STB_N before and after interrupt,they are all normal.

The exceptions are TX and RX. RX garbled code, TX not returned after communication interruption

 

0 Kudos
1 Reply

102 Views
guoweisun
NXP TechSupport
NXP TechSupport

在您的case回复过了!